STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! EMMC Compatibility with STM32H757XIH6

Please suggest recommended values for EMMC for the following parameters:Max Read/ Write speed supportedWhat is maximum memory density it can support?What is the bus width it can support?Any recommended NAND based EMMC part number of memory density 16...

USBX ThreadX doesn't recognize device attached

I'm trying to implement the USBX Audio class using the board STM32U5A9J-DK and the USBC port present on the board.I've opened the default project from TouchGFX selecting the ThreadX one. I then opened the .ioc file in the CubeMX and activated the USB...

nico23 by Senior III
  • 2263 Views
  • 7 replies
  • 0 kudos

STM32F205RG RTC Problem.

Greetings,I have connected external crystal of 32.768 KHz to STM32F205RG for RTC time keeping purpose. I have also enabled RTC output on pin PC13. Below is my code for RTC Initialization ...int main(void) { /* USER CODE BEGIN 1 */ /* USER CODE E...

about the question of MFG label change

Hello,  is there any changes about  MFG label of the STM32 MCUs products ?we receive the new DC product, and found the "Assembled in: Site" was miss ,which shall be show on the second line of the label, pls check below photos , is it correct ?if yes ...

ViviXia_0-1750815735807.png
ViviXia by Associate
  • 639 Views
  • 1 replies
  • 0 kudos

STM32H743II : Timer Frequency Tolerance

Hello,I am working on creating a timer function using the timer peripheral of the STM32H743II, with a timer range from 1 second to 3600 seconds.I'd like to ask a question regarding the frequency accuracy of the timer.Let me first explain the current ...

keiju_0-1751263133451.png keiju_1-1751263178392.png
keiju by Associate
  • 659 Views
  • 1 replies
  • 1 kudos

RTC as wakeup-source on C0 family

Hello, I have found various guides on how to configure the RTC as wakeup-source. However, they do not seem to apply to the C0 family.In the CubeIDE I cannot find the depicted settings on RTC, (most notably, no option to select internal wakeup and con...

Panda by Associate III
  • 2602 Views
  • 10 replies
  • 4 kudos

Resolved! STM32L433RCT VDD12 pins - what should I do with them ?

I am using the NUCLEO-L433RC-P development board and in the process of designing my own PCB.But I am unsure what to do with the VDD12 pinsOn the NUCLEO-L433RC-P development board they are connected to an SMPS using an analogue switch.If I dont use an...

freeflyer_0-1751227979437.png

Missing section IRTIM in STM32U0 RM and more.

1. According to datasheet, STM32U0 family have an IRTIM (Infrared interface). But this section is missing in RM0503. Also in SYSCFG_CFGR1 there is missing IR_MOD and IR_POL bits.2. In RTC section Figure 297 it is missing RTC_OUT2 and RTC_REFIN pins. ...

AA1 by Senior III
  • 7899 Views
  • 18 replies
  • 4 kudos