User Activity

New question from this thread. So in order to use both SMPS and LDO, given in board schematics,I mounted SB6 and SB17 (SB44, SB46, L4 already mounted)and removed SB5 and SB18 (rest already not mounted).After than i flashed it with keeping the followi...
New question moved from this original thread. Thanks for the quick response.So basically the HW is configured in SMPS. So in order to obtain 480MHz, what changes should i do to the hardware. Or is there any way i could do it without changing the hard...
I tried flashing a project created for the STM32H745I-DISCO board in CubeMx. I configured clock speed for the M7 core to 480MHz and the M4 core speed to 240MHz. After flashing, if i disconnect the board, the deadlock occurs. Then i have to pull up th...
Kudos given to