2025-02-03 5:37 AM - last edited on 2026-01-24 11:29 AM by mƎALLEm
Can anyone comment on the prologue and epilogue of following CM7 code, particularly the content of r7 when the routine returns?
{
0: b480 push {r7}
2: af00 add r7, sp, #0
if ((ANADIG_MISC->MISC_DIFPROG & ANADIG_MISC_MISC_DIFPROG_CHIPID(0x10U)) != 0U)
4: 4b0b ldr r3, [pc, #44] @ (34 <RamBased_ROM_API_Init+0x34>)
6: f8d3 3800 ldr.w r3, [r3, #2048] @ 0x800
a: f003 0310 and.w r3, r3, #16
e: 2b00 cmp r3, #0
10: d005 beq.n 1e <RamBased_ROM_API_Init+0x1e>
{
g_bootloaderTree = ((bootloader_api_entry_t *)*(uint32_t *)0x0021001cU);
12: 4b09 ldr r3, [pc, #36] @ (38 <RamBased_ROM_API_Init+0x38>)
14: 681b ldr r3, [r3, #0]
16: 461a mov r2, r3
18: 4b08 ldr r3, [pc, #32] @ (3c <RamBased_ROM_API_Init+0x3c>)
1a: 601a str r2, [r3, #0]
}
else
{
g_bootloaderTree = ((bootloader_api_entry_t *)*(uint32_t *)0x0020001cU);
}
}
1c: e004 b.n 28 <RamBased_ROM_API_Init+0x28>
g_bootloaderTree = ((bootloader_api_entry_t *)*(uint32_t *)0x0020001cU);
1e: 4b08 ldr r3, [pc, #32] @ (40 <RamBased_ROM_API_Init+0x40>)
20: 681b ldr r3, [r3, #0]
22: 461a mov r2, r3
24: 4b05 ldr r3, [pc, #20] @ (3c <RamBased_ROM_API_Init+0x3c>)
26: 601a str r2, [r3, #0]
}
28: bf00 nop
2a: 46bd mov sp, r7
2c: f85d 7b04 ldr.w r7, [sp], #4
30: 4770 bx lr
32: bf00 nop
34: 40c84000 .word 0x40c84000
38: 0021001c .word 0x0021001c
3c: 80981070 .word 0x80981070
40: 0020001c .word 0x0020001c
Thanks very much!