STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! jlink fails to connect to stm32n6

Hey All,I hope you can help me. I'm trying to bring up my new board, which contains a STM32N657IO. Attached are the schematics. You can assume the 5V supply is working(it is after a few bodge wires). My problem is as follows. I'm trying to connect to...

robojan_0-1751191134229.png
robojan by Associate
  • 2624 Views
  • 2 replies
  • 1 kudos

USB EMI Filter - USBUF01W6

Hello Friends,I am Using STM32F303 MCU for my FULL Speed USB  communication board. Used interrupt transfer.Board is going to use in Noisy Industrial environment.So , Planned to use Shielded USB cable with EMI Chokes ( Both Side ).Cable Length is 1.8 ...

bsuthar by Senior
  • 1380 Views
  • 7 replies
  • 0 kudos

Resolved! Unexpected results with iterative use of STM32H5 CRC unit

Hi,I am trying to use the STM32H5 CRC unit via HAL to calculate a CRC32 (ISO-HDLC) over multiple chunks.This works correctly via:hcrc.Instance = CRC; hcrc.Init.DefaultPolynomialUse = DEFAULT_POLYNOMIAL_ENABLE; hcrc.Init.DefaultInitValueUse = DEFAULT_...

MFuch.3 by Associate II
  • 1653 Views
  • 6 replies
  • 3 kudos

STM32F446RET6 Virtual Com Port

I’m working on a custom board with an STM32F446REt6 and a USB Type-C 2.0 connector (GCT SB4105-GF-A). I haven’t implemented any external pull-up on the D+ and D- lines, but on the CC1 and CC2 pins I have 5.1k pulldown resistors. I managed to load the...

Screenshot 2025-07-01 163936.png
Nik_01 by Associate
  • 994 Views
  • 1 replies
  • 0 kudos

Resolved! Comparator to encoder configuration?

I want to route the internal comparators on the STM32G0B1 to the inputs of the encoder module. I can't find a way to do this in CubeMX. When I select "Encoder Mode" in the timer configuration, there is no option to route the comparators to the timer....

WA by Associate
  • 1379 Views
  • 3 replies
  • 2 kudos

Resolved! Stm32f407vgtx TIM output compare mode

Hi I am trying to achieve output compare mode in TIM1 in stm32f407vgtx board . I am trying to generate a delay of one ms and running a timer clock at 1mhz after divide it with prescaler. I have enabled upcounter,TIM_CCER_CC1E bit in CCER, TIM_EGR_CC1...

Ash1 by Associate III
  • 1086 Views
  • 1 replies
  • 0 kudos