User Activity

Hello!I'm trying to use an external SDRAM (IS42S16320F) with an STM32H753 but no luck till now.Could please anyone check if my settings are correct because I don't know if I made a bug here.  For that I have attached the FMC configuration and the sch...
Hello!I have my custom board with STM32F767 and external SDRAM (MT48LC4M32B2 - 128MBit) on it.Basically the connection between them works fine, because I'm able to write and to readout the data. The problem is, that if I try to access an address abov...
Hi!I'm using a custom PCB with STM32F767 on it with LAN8742a for Ethernet communication.Just to mention, I'm totally new to Ethernet topics.I have already search for an very simple example on how to just test the connection from the STM to LAN8742a (...
Hello!I'm using a custom board with STM32F767 and external Flash memory connected to the QSPI (MX25L12835F).I want to create a simple test, where I read and write some data into the external Flash.In the first shot I want to use the normal SPI mode t...
Hello!I'm using the Cube IDE with STM32H753 and trying to initialize the LTDC from HAL.I already did this with success for the STM32F767.But for the STM32H753 I have some problems with LTDC drivers.The programm hangs up during debugging on the automa...
Kudos from