STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

On STM32h753 UART interrupt is working fine after programming the controller using keil but malfunctions after complete power reset ?

I am working on STM32H753 microcontroller. I want to receive string using UART interrupt and send the same string back on UART. The IDE is keil uvision 5. The problem I am facing is that when I first program the MCU UART is working fine and I am rece...

0693W000007EthkQAC.png
Akash_k by Associate III
  • 1635 Views
  • 2 replies
  • 0 kudos

About DFSDM filter configurations FOSR and IOSR

When I increase the value of FOSR and IOSR,Iam ​not getting the proper values output from the dfsdm filter it keeps varying and is not also proper HAL_DFSDM_FILTERREGULARSTARTDMA(&hdfsdm1_filter0) ​​H​ow to keep the values of FOSR and IOSR?

No STM32 Target Found - custom board

Hi guys, I'm starting from a bare STM32G070KB, and cannot for the life of me get it to connect.I had this problem with an STM32G071CB but was able to solve it. The problem I was having was that I couldn't get an ST-Link to read the chip on a breadboa...

UMoha.1 by Associate
  • 993 Views
  • 1 replies
  • 0 kudos

STM32F050C4T6A I want to use as a drop in replacement since I cannot find stock in the STM32F030C8T6 When I installed it in my board I use two I2C ports and they both work but the manual says there is only 1 I2C port. Am I ok to use this chip?

STM32F050C4T6A I want to use as a drop in replacement since I cannot find stock in the STM32F030C8T6 When I installed it in my board I use two I2C ports and they both work but the manual says there is only 1 I2C port. Am I ok to use this chip going f...

RScam.1 by Associate
  • 1422 Views
  • 1 replies
  • 0 kudos

Data from ADC (DMA) over UART (DMA)

Hi,I am trying to perform continuous ADC conversions from a microphone using DMA, save that data to a large buffer, and then transmit that data using Uart (DMA). I have successfully setup the ADC to perform the DMA conversions along with saving them...

kcire L. by Associate III
  • 4272 Views
  • 3 replies
  • 0 kudos

I2C Slave endless clock streching

Hi, I have the problem that I get an endless slave Clockstretching.STM32F072 I2C configured with CubeMX, Primary slave adress $32If I fire a Tx frame from a master with for example:HAL_I2C_Master_Transmit(&hi2c1, 0x64, buf, 1, HAL_MAX_DELAY);The cloc...

0693W000008Fz3wQAC.jpg
RNaas by Associate
  • 778 Views
  • 1 replies
  • 0 kudos

Resolved! Put interrupt in RAM or pre cache

Hello,I am using GCC and eclipse CDT. I need to execute an external interrupt very fast (every 4µs). There is not a lot to do in there but I use about 2.5µs of time in the interrupthandler. I tryied to put the handler in to ram wich gave me the reloc...

Standby current is sometimes to high STM32L151CBT6A

We switch several times the µC into Standby Mode and the current is as described in the specification.But sometimes over the Vdda Pin the current is 1mA. We switch adc/dac vrefint etc off. No BOR in use.We checked each Ports, but the current is comi...

ADC value not able to read.

Hi, i got a fan failure project . For that i need to select 2 adc channels in DMA mode for rms calculation , and 2 digital input for my powerfactor reading . here i am using AC (230Vac) and DC (5v) supply both .I select two timers with 100khz in...

Lchal.1 by Associate III
  • 2120 Views
  • 0 replies
  • 0 kudos

Is there a compile time conditional statement for debugging?

Hello everyone! I am trying to debug some code but there are some flags in flash that keep getting set when I exit debug and it enters run mode (or when I power up the sensor. Basically, anytime it gets a chance to run before I can get it in debug ...

JayDev by Senior II
  • 1279 Views
  • 2 replies
  • 0 kudos