STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Nucleo-L476RG - SD card not creating any .txt files or any files at all. Does anyone have an example code to let the sd card work ?

Hey guys,I am pretty new to stm32 (-> beginner) and I am trying to create a .txt file on my sd card. My pc is connected by usb to the Nucleo-L476RG board, which is connected to an onboard sd card.These are the connected pins:   /**SDMMC1 GPIO Configu...

TNguy.9 by Associate II
  • 5983 Views
  • 12 replies
  • 0 kudos

Undefined reference to HAL_UART_Init

Anyone knows how to fix undefined reference to HAL_UART_Init,HAL_UART_receiveI included all necessary files for this but somehow it doesn't find any reference#include "stm32f4xx_hal.h" #include "stm32f4xx_hal_conf.h" #include "usb_device.h" #include ...

arduo by Senior
  • 12881 Views
  • 11 replies
  • 1 kudos

How to use USART RTO timeout?

I have a STM32L4xx series microcontroller. My goal is to use RTO in USART to issue a timeout, from the time a read was attempted (not only from the last stop bit). This is needed as its possible for nothing to be received. How do I acheive this using...

Accessing outside flash area is working...

Tested to flash a 128k (STM32F105) device with a firmware (40k) that is compiled for 256k and it works. Even when the firmware reads and writes data (config) to address location 0x0083E000 which is way out of the 128k device memory area.Is there some...

HHaga.1 by Associate
  • 1421 Views
  • 3 replies
  • 0 kudos

Experiences with STM32 and XRay or CT

Hello,during qualification tests, our design with STM32 L4 first went through XRay tests and afterwards even CT to check for soldering problems etc.XRay was fine, but we have an issue with CT were the controller quit function afterwards. Not even a J...

RHaag.1 by Associate II
  • 2461 Views
  • 5 replies
  • 0 kudos

STM32 ADC acquisition after some amplification block

Hi, I have a random amplitude signal with 10 us period, coming from DAC channel 1 of the STM32 connected to some block with amplifier and switches. The block is finally connected to an input channel of the ADC within the STM32. The block ...

VKuma.11 by Associate
  • 923 Views
  • 1 replies
  • 0 kudos

Resolved! STM32G070RB HSI16 Clock and clock calibration issues. Is there a clock calibration example without the need to use HSE or LSE clocks?

I am trying to acquire the amount of ticks a timer counts using a 50Hz signal (acquired from the mains using hardware). For this I use a EXTI8 interrupt where the 50Hz signal is sampled. I can see on the scope that this interrupts works perfectly (by...

CP.Tang by Associate II
  • 3159 Views
  • 5 replies
  • 0 kudos