cancel
Showing results for 
Search instead for 
Did you mean: 

Looking for a development board which support 32bit data Size in SPI Mode

PPand.4
Associate II

Hi,

I am looking for board which support 32bit data size in SPI Mode. I found NUCLEO-H743ZI2(https://www.st.com/en/evaluation-tools/nucleo-h743zi.html) development board but not very clear that it will support 32bit data size in SPI Mode or not.   As per board datasheet(https://www.st.com/content/ccc/resource/technical/document/datasheet/group3/23/be/db/eb/29/39/4b/eb/DM00387108/files/DM00387108.pdf/jcr:content/translations/en.DM00387108.pdf) "Three standard I2S interfaces (multiplexed with SPI1, SPI2 and SPI3) are available. They can be operated in Master or Slave mode, in Simplex communication modes, and can be configured to operate with a 16-/32-bit resolution as an input or output channel".  

Kindly request you to please confirm that this NUCLEO-H743ZI2 development board will support 32bit data size in SPI mode? If not kindly please

suggest any other available development board which support 32bit data size in SPI mode.

Regards,

Pankaj Pandey

This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
TDK
Super User

Usually this is not an issue since you can simply send multiple bytes to get a 32-bit frame. But yes, this can operate in native 32-bit frame by configuring SPI_CFG1_DSIZE appropriately.

The reference manual is a better source of information about how the peripherals operate than the datasheet.

https://www.st.com/resource/en/reference_manual/dm00314099-stm32h742-stm32h743-753-and-stm32h750-value-line-advanced-arm-based-32-bit-mcus-stmicroelectronics.pdf

If you feel a post has answered your question, please click "Accept as Solution".
PPand.4
Associate II

Hi TDK,

Thank you for quick response and update. I will go through the datasheet, for NUCLEO-H743ZI2 I am reading SPI demo example from this link(https://github.com/STMicroelectronics/STM32CubeH7/blob/master/Projects/NUCLEO-H743ZI/Examples/SPI/SPI_FullDuplex_ComPolling/Src/main.c) where I found SPI data size is set for 8bit (SPI_DATASIZE_8BIT). Now I want to test this demo program for 32bit , for that I need to change this macro from 8bit to 32bit(SPI_DATASIZE_32BIT). So now question is this that above change is enough to test SPI demo program for 32bit data size ? or any further changes are require to test 32bit data size ?

TIA!!

Regards,

Pankaj Pandey

TDK
Super User

I would imagine that would change the frame size, but other changes to the transmit and receive function would be needed to ensure your buffers do not overrun.

If you feel a post has answered your question, please click "Accept as Solution".