User Activity

We have used the I2S and DMA function.​
​Could we create a hi-fi audio project base on STM32L series?What series can be used?​​
We need to transmit and receive I2S data at the same time.​But we can’t transmit and receive at the same time now.Then we want to know whether the SAI of STM32L433 can achieve features similar to full-duplex?If yes, is this setting correct?​​​
Could we used the SPI interface control the 5V LED Driver IC?STM32L412's VCC is 3.3V, SPI's pins are FT_f type.LED Driver IC's VCC is 5V.Is there anything that needs extra attention?Will there be problems with SPI operation?​