STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32H747 with OV5460 low frame rate

I am using STM32H747 MCU with OV5460 camera. The FPS i got from the camera is around12-13 fps is that any method to increase the frame rate.I tried by increase PLL clock but there is no image received.Thanks

KHowe by Associate II
  • 1471 Views
  • 4 replies
  • 0 kudos

Resolved! DSI Host interrupt and status register 0 (DSI_ISR0)

Hello,We are currently using a STM32U5G9 with MIPI Port 2 lanes talking to ST7701S TFT driver. We found on power up when we have a lot of error in DSI_ISR0.PE3 and DSI_ISR0.PE4 are set, display do not start. Definition of this error is : This bit ind...

cr_qc by Associate II
  • 665 Views
  • 2 replies
  • 0 kudos

ULPI integration on stm32 mcu clock reference

Hi everyone,we are moving our design from usb full speed to usb high speed using STM32F76VI.We want to use the suggested module STULPI01A in order to achieve this.On datasheet is specified to use a precise reference clock.Since our application use a ...

Comp1 blanking not working inverted input

Hi,While working on the code for an STM32H7B0, I'm having issues with the blanking function of COMP1. Specifically, it works correctly when the comparator is in non-inverting mode, but if I invert the comparator's output (to detect falling thresholds...

garinus_0-1747737757678.png
garinus by Associate II
  • 866 Views
  • 1 replies
  • 0 kudos

Resolved! STM32H563 MD5 Hash Support

Trying to get MD5 hash acceleration working on the Nucleo-H563Zi. I can get SHA1 hash engine to work via bootstrapping a project via CubeMX, but for some reason MD5 is not a selectable option for the hashing algorithm in CubeMX.  All other algorithms...

Resolved! stm32L100 can not access flash (0x8000000)

Moved from MPUs section - STM32L100 is an MCU, not an MPUI compare this my layout board (with outer st-linkv2 connected), and stm32l100c disco.stm32l100c disco does not have such a question. It will show "Error 57: Illegal Address(0x8000000)".And I d...

2284530.jpg
huang by Associate
  • 1053 Views
  • 2 replies
  • 1 kudos