User Activity

hi question how can I read a 4 channel encoder with stm32 EA +,EA -,EB+,EB-?
Hi, I'm giving the example of the two stm32 boards at this linkhttps://github.com/sogongbang/STM32CubeF4/tree/master/Projects/STM32F4-Discovery/Examples/I2C/I2C_TwoBoards_ComPollingI made and copied the connection and the code then I checked several ...
Hi I wanted to translate the following Arduino code with hal stm:uint32_t TMC5160_SPI::readRegister(uint8_t address){// request the read for the address_beginTransaction();_spi->transfer(address);_spi->transfer(0x00);_spi->transfer(0x00);_spi->transf...
Hi, I'm reading up on stm mp1, in particular the Linux side, my intent was to use the M4 to read data from sensors and transfer them to the A7 on the Linux side. Now I've read the function in C code that reads the messages from the manual: read:int r...
Hi i 'm using stm32  mp1 can i tale autput message from cat /dev/tty/mesg  and store data from cortex m4,i want to write code in c with to store autput cat,for example everytime che come a message from m4 interrupt trigged and store data thanks