User Activity

Can someone help me how to use one interrupt pin for Activity/Inactivity and another for Free Fall detection? I need to use it in the lowest possible possible mode as my device is coin cell battery powered.Regards,Asish Banerjee
Hello,I am facing problem with task switching in FreeRTOS. I am using my custom board with STM32L476RC running at 80 MHz clock. Using STM32CubeIDE and configured project using CubeMX. I am using 3 tasks. Task 1 has some functions which uses osDelay ...
Hello,I am trying to read single ADC channel using NUCLEO-H743ZI2 board but the result is wrong. I have created a very simple project using CubeMX. Kept the default Clock setting. Enabled ADC3 CH0 (PC3_C Pint) in single ended mode polling. Enabled UA...
Kudos given to