STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

The question about Sleep mode

​I want to let STM32L552CC into sleep mode.I add HAL_PWR_EnterSLEEPMode(PWR_MAINREGULATOR_ON, PWR_SLEEPENTRY_WFI);Build is OK,but when Debug ,the error appeared, Why?

0693W000008vsgHQAQ.png
XZou.1 by Associate II
  • 1304 Views
  • 2 replies
  • 0 kudos

Have the Board

Hello, I will take place at the training at the 25th and own already the board.Thanks for providing this workshop!Best regards

CSomm.2 by Associate
  • 817 Views
  • 1 replies
  • 0 kudos

Resolved! Confusing behavior of __asm__ __volatile__("nop")

Hello dear ST-Community,I'm currently working on a 8-Bit interface for a TFT-Display. I'm using a STM32F405RGT6 for the Project.While debugging a timing issue i ran into, I found an interesting behavior when using __asm__ __volatile__("nop") for ns-s...

JHöfl.1 by Associate III
  • 7297 Views
  • 6 replies
  • 0 kudos

How to manually enabling NVIC irq for timer6 in STM42F407

Hello, i have written the following code for interrupt delay based on timer as shown in the attached fileBut Keil shows the error bellow on the line.Why it gives me such error,how do i manually enable the IRQ of TIM6?Thanks, NVIC_EnableIRQ(TIM6_IRQ...

Nbkjh.1 by Associate II
  • 3190 Views
  • 3 replies
  • 2 kudos

Hi, I have the board and not received any confirmation

 Hi, I have the board and not received any confirmation (teams invitation) or confirmation, just the initial email. I have emailed tilen.majerle@st.com from the company email account but have gotten no response. I tried to book again however your sys...

Ahmed by Associate III
  • 1077 Views
  • 1 replies
  • 0 kudos

Resolved! How accurate is ST VREFINT Calibration?

I am using STM32F030F4P6. VREFINT is supposed to be calibrated at 3.3v +/- 10mV and 30 degrees C. In my application the VREFINT calibration value is 1543 meaning the reference voltage is 1.243V (3.3/4096*1543) this is on the high end of the spectru...

mp035 by Associate III
  • 11662 Views
  • 12 replies
  • 2 kudos