User Activity

Dear All,Am converting one code from HAL Library to SPL Library.In same am using SPI BUS , for it one of function is used which is as mentioned below:-" HAL_SPI_Transmit(&_W25QXX_SPI,pBuffer,NumByteToWrite_up_to_PageSize,100); "Same i wanted to conve...
Dear All, Am writing code for Winbond Memory chip "w25q64", for same i got some reference from git hub , but it is with HAL library, same i am converting to standard peripheral library.HAL_SPI_Transmit(&_W25QXX_SPI,pBuffer,NumByteToWrite_up_to_PageSi...
I need what max size sd card i can connect to DIscovery Board containing Stm32f07d Controller over SPI?As am planning to take that reference in my design.And what is the solution to interface sd card of 8GB Size over SPI in Stm32f072 Controller?Also ...
Hi all, Can somebody support in getting datasheet of "324 ST MZCS903" which is a 14 - pin chip.Am unable to get from internet .Thanks in advance.Rohitrohit.kadecha@battrixx.com
Kudos from