STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

i2c implementation between MCU and sensor

I would like to read temperature and humidity values from TI HDC2080 sensor when using STM32L0F4 MCU. Programming language is C and environment is CubeIDE. I downloaded sensor library from dev.ti which includes a file where MCU specific I2C functions...

0693W000008yPHbQAM.png
Indois by Associate II
  • 746 Views
  • 0 replies
  • 0 kudos

I am trying to read Vbat(battery voltage) using ADC in STM32F042 ,the reading always is Zero. Anyone please find the reason for it.The code is as follows..please dont metion the syntax error ..i have copied only the necessary parts

void HAL_ADC_ConvCpltCallback(ADC_HandleTypeDef* hadc){ if(__HAL_ADC_GET_FLAG(hadc,ADC_FLAG_EOC)){ adc_value=HAL_ADC_GetValue(hadc); }}main(){ HAL_ADC_Start_IT(&hadc); while(1) { }}static void MX_ADC_Init(void){ ADC_ChannelConfTypeDef sConfig =...

RR.7 by Associate II
  • 867 Views
  • 0 replies
  • 0 kudos

STM32H7xx I2C driver with DMA not working

Hello,i use STM32CubeIDE with FW 1.60 with and want to use the I2C driver with DMA to read and write some data do a device.I configured it properly in CubeMX and the code has been generated and all interrupts etc. are implemented.When i test it with ...

CKörn.2 by Associate II
  • 920 Views
  • 0 replies
  • 0 kudos

Resolved! DFU - FAIL VERIFY - 8 byte align magic...

Posted on February 13, 2017 at 21:45So I'm DFU'ing. Successfully bootloading the device with the USB connections on PA11 and PA12 DFU is built into the STM32L476. Plodding along and loading my micro a few times with a few different compilations all ...