STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Measuring DC current with ACS271(20A)

Hi everyone,I am too new at STM, so I couldn't understand how to measure DC current. Can anyone help me to do my setting and code, please. I found out code for AC current and I decided to change some parts of this code, but I couldn't understand how ...

MÇETİ.1 by Associate III
  • 1750 Views
  • 2 replies
  • 0 kudos

Reading multiple channels of ADC with DMA STM32F40

I am working on an old code written by someone. The application requires reading 13 ADC channels roughly at 8k samples per second. The read values are written in two buffers in double buffer mode (4096 each).The ADC is implemented in scan mode with t...

NKunwar by Associate II
  • 789 Views
  • 0 replies
  • 0 kudos

SPI slave not always sending data

Hi,I'm using an STM32F429 Discovery board and having an issue with the FW_F4_V1.25.2 firmware. I have SPI3 configured as a full-duplex slave (currently used only to send) which sends data out to a Beaglebone as a Master. The Beagle supplies a 16MHz c...

SSmit.0 by Associate II
  • 3608 Views
  • 6 replies
  • 0 kudos

mXT336T driver for stm32

I'm trying to write driver code for stm32 of maxtouch MXT336T chip starting from Linux driver found here https://github.com/atmel-maxtouch/mxt-appIs this path more efficient than rewriting the all driver starting from the datasheet?Any idea?Has someb...

SD'An.1 by Associate
  • 1909 Views
  • 1 replies
  • 1 kudos

STM32L151CBU6 Firmware Download problem

Hi, everyoneI, Currently STM32L151CBU6 is in use.The firmware uses a .HEX file,I am using the firmware download to change the boot mode.Now, firmware download through STM FlashLoader Demo.exe(2.8.0) works normally.However, STMFlashLoader.exe is used ...

Jyoun.1 by Associate
  • 1222 Views
  • 1 replies
  • 0 kudos