STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Log numeric data in SWV ITM Data Console

Is it possible to customize the display format of ITM data in the "SWV ITM Data Console" view to show the raw data values, rather than the text interpretation?For example, I'm writing various counter values to different ITM ports, and would like a co...

0693W000007EEUpQAO.png 0693W000007EEUuQAO.png
Miles1 by Associate III
  • 1778 Views
  • 1 replies
  • 3 kudos

Timer Input randomly skips interrupt.

I'm sertanly missing something.I have a board with STM32F103 that control fan via PWM and have to check it's speed with Fan's TACH out. TACH out is consistent PWM signal with duty cicle 50% and frequency 80 Hz.Chip is running with 64MHz clock, APB1 i...

0693W000008yz12QAA.png
viteo by Associate II
  • 3976 Views
  • 7 replies
  • 0 kudos

STM32H745 Nucleo: ADC with DMA don't work

Hi! I have STM32H745 Nucleo and i want to transfer data from ADC via DMA.1. At first i write code for ADC with out DMA (ADC3, PF10 in) and it work excellent. I get positive knovlege.2. At second step i tried to use DMA (DMA1 stream 1), but code don't...

AAnt.1 by Associate II
  • 2020 Views
  • 4 replies
  • 0 kudos

Resolved! Compatible MCU among stm32f4 series

Hi, everyone. I am Emily.​ I would like to know the MCU which is compatible to 'stm32f446RET'.​Also I wanna double-check the possiblity of compatible usage between 'stm32f407VET'​ and 'stm32f417VET'.​Please help me:crying_face:​

EHa.1 by Associate II
  • 2475 Views
  • 3 replies
  • 0 kudos

[X-cube-AI] Does stm32 F/H arm coretex-M7 series hardware has TPU(tensor processing unit) for hardware accelation ?

Hello. I want to know does stm32 cortex m7 series has TPU (tensor processing unit) for hardware acceleration. I heard that TPU has a systolic array which is a network of processors that are responsible for performing computations and passing the resu...

0693W000008ywRRQAY.jpg
Yjang.1 by Associate II
  • 3665 Views
  • 4 replies
  • 0 kudos