User Activity

Hi All, I'm currently working on a project where I will have a proxy/Friend Node that will talk with a Low power Node.The proxy node should be able to go on standby when requested and in the condition I would like to obtain the optimal current consum...
Hi All, I'm currently using an STM32WB5MMG module on two devices to establish a Zigbee connection between them.My project is based on the example called "BLE_Zigbee_Dyn"(one device should also be able t communicate using BLE ) implementing everything...
Hi All, I'm currently working on a project that uses the STM32WB5MMG module.I did a porting of one of the examples of the repository (BLE_Zigbee_Dyn) for RTOS and everything is working fine.Now I'm trying to put the MCU in STOPMODE2; a GPIO Interrupt...
Hello guys, I'm currently working on a STM32WB55VGY and I have some problem setting up the Zigbee network.Using the example I found in the repository I was able to create a simple Zigbee network using the preconfiguredLinkKey.Now I would like to go f...
Hi,I'm currently having a problem with the STM32CubeIDE software after updating it to 1.6.0.Trying to compile a project I noticed that the final dimension in flash increase about 2000bytes.The problem is that I found this because one of my projects n...
Kudos from