STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Flash Loader Demonstrator cannot open port

I have a Win10 notebook computer. When I run the Flash Loader Demonstrator, it correctly finds the com port being used (the only one) but when I click 'Next' it always says ​"Cannot open the com port, the port may be used by another application". Thi...

MBeal.1 by Associate
  • 4998 Views
  • 3 replies
  • 0 kudos

SDIO fail to run over freq > 2MHz

Hello Everyone !I am using 4bit SDIO over STM32 F4 Nucleo board (STM32F412ZG).I am facing issue when running higher SDIO_CK clock.When I use smaller 'Div' value (higher freq), it does not produce correct clock and in stead produces very small clock i...

YMant.1 by Associate II
  • 3221 Views
  • 5 replies
  • 0 kudos

Resolved! CubeMX / STM32L476 / NAND Flash

I'm trying to experiment with a NAND flash connected to a STM32L476VG and I'm using CubeMX to set everything up. No matter what I do, I cannot get CubeMX to show me a NAND flash as an option for the FMC. The options are LCD, Muxed NOR and Muxed PSRAM...

MNesd.1 by Associate
  • 2392 Views
  • 3 replies
  • 0 kudos

STM32H743 nucleo won't work in USB OTG FS

Posted on November 07, 2017 at 10:49Hello,I am working on a STM32H743 – NUCLEO 144 and need to use OTG_FS device only option in CDC mode.I generated a project using the stm32cubeMX and have defined: SYS – Time bases : TIM1USB DEVICE – class f...

Resolved! STM32F, L, W, H, U series version keyword.

Hi, guys.​STM32 have a several series STM32F, STM32L, W, U, H..., but what is the meaning of F, L, W, H?(like a F: fast, L: large, H: high spec...?)I think this work is just an version number, someone know is it?Thank you.