STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

HardFault PRECISERR using FDCAN1

Good morning,Im using the CAN-Module of STM32H743 NUCLEO board and so far I'm quite happy with it. But now I ran in to this hard fault error which seems to occur at a random point in time, but it will appear sooner or later. Using the built in Fault ...

MLang.7 by Associate III
  • 2015 Views
  • 2 replies
  • 0 kudos

Resolved! Setting up TIM8 strange issue

Hi All,I am setting up TIM8 CH1 and CH3 on a STM32G431 and am seeing a strange result. First of all, I am using an external signal coming in on PC6 TIM8 CH1. For TIM8 CH3 I am only using a software trigger internal to the MCU, I'm not using any exter...

BTrem.1 by Senior II
  • 2045 Views
  • 2 replies
  • 0 kudos

How to checkif an EEPROM exists at I²C?

Hello!I'm trying to detect if a removable EEPROM exists in a given system, but I ran into some problems.With configuration  STM_enableRCCAPB1PeriphClock( RCC_APB1Periph_I2C1, ENABLE ); STM_resetRCCAPB1PeriphCmd( RCC_APB1Periph_I2C1, DISABLE ); I2C_Cm...

KSchü.2 by Associate II
  • 2076 Views
  • 3 replies
  • 0 kudos

Resolved! Issues trying to get USART writing to a console. It only works when I have stlink connected. As soon as I disconnect stlink the output stops. The output does seem to go through USART2_TX (PA9) as disconnecting it stops the output

I am using STM32L010F4 20 pin on a simple breakout board.I am running STM32CubeIde and using a STM32Lc100-disco as my programmer via SYS_SWCLK (PA14), SYS_SWDIO (PA13) and NRST.All works well can get SPI etc running no problem.I mapped USART2_RX to P...

Jdu P.1 by Associate
  • 1532 Views
  • 2 replies
  • 0 kudos

Interrupt management

I would like to create a kind of calendar with one STM32 MC. When the application will advise me to do scheduled activities. I was thinking to use timer interrupt and I would like to know if there is a quantity limitation of timer interrupt per STM32...

Wdowa.1 by Associate II
  • 1093 Views
  • 1 replies
  • 0 kudos

Is This Read Disturb Effect of STM32F4?

Hi, dear sir or madam in team,In my project, I use STM32F407VGT6 as CPU for a digital control power supply. I use one sector (not the last sector) of flash memory for storing some constant conversion coefficients for ADC. (There are more than 13 conv...

JYou.4 by Associate
  • 1138 Views
  • 1 replies
  • 0 kudos

Resolved! Does stm32f4 or h7 have DSP hardware implementation?

Hey guys.There is a library named cmsis_dsp for these mcus but when i took a look inside them there were just simple codes and not hardware implementation of dsp.But in datasheet it says:The STM32F405xx and STM32F407xx family is based on the high-per...

Resolved! D-shot with STM32F765: timer + pwm + dma

Hi all,I have a STM32F765, which i want to use to generate 4 D-shot signals on 4 GPIO, in the specific 4 gpio connected to Timer 1 .The timer is set as 4 channel pwm with DMA (memory to perpheral).The issue is that i'm able to generate the desired si...

0693W00000AMvOnQAL.png
Pmica.1 by Associate II
  • 7653 Views
  • 9 replies
  • 1 kudos

Resolved! How to receive UART data STM32F103 using interrupt mode?

I am using STM32CubeIDE with a STM32F103 and have UART1 setup in interrupt mode. Is there a working code example anywhere that tells how to implement UART interrupt mode? I have been unable to find via g~~gle. I have worked with multiple other proces...