2021-01-05 7:23 AM
Hello.
Is it possible to use hardware SPI with STM32G030J6M6 (SO-8)?
SPI1 use PA1 (NRST pin) for CLK without remap possibility.
SPI2 also use PA1 (NRST pin) for CLK, but has CLK remap to PC14. In that case no MOSI pin.
I try to use SPI1. PA1 configured as AF0 PP.
Writing to the SPI1->DR register results in a reboot.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.