STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Can a Timer Capture Compare be skipped if needed?

I'm using a Timer (TIM8) in a capture compare application for measuring timing between signals. In some cases I don't need the value so I have been skipping the read of the CCRx register. I'm using a HAL command as the code below shows:The HAL_TIM_R...

BTrem.1 by Senior II
  • 1287 Views
  • 2 replies
  • 0 kudos

How to read VBATT Voltage from ADC

I Am using STM32F303CB.I want to read the VBATT voltage from ADC1_IN17 as VBATT is connected to ADC1 channel 17.Here my Code:void ADC1_Init(){   RCC->CFGR2 |= RCC_CFGR2_ADCPRE12_DIV1;   RCC->AHBENR |= RCC_AHBENR_ADC12EN;   RCC->AHBENR |= RCC_AHBENR_G...

STMH753 GPIO port pin read is slower compared to the STMF429

Hi,I am porting an application from the STMF429ZI to the STMH753ZI and have noticed that the STMH753 is slower when reading the GPIO inputs compared to the STMF429. In one function, multiple GPIOs are read to gather 16 input states. Measuring this fu...

TSosi.1 by Associate III
  • 1995 Views
  • 1 replies
  • 0 kudos

Resolved! DALI Interface for STM32G MCU

Hi,I am planning to implement DALI on STM32G MCU, I have looked at the documentation but all the example projects are with STM32L1 or STM32F1 and the library provided by STM is based on IAR workbench. My questions are Can I implement DALI Slave on ST...

KPras.1 by Associate
  • 2085 Views
  • 1 replies
  • 0 kudos

STM32F4 SDRAM & NOR FLASH READ WRITE PROBLEM

I am troubling to write and read data from external SDRAM & NOR Flash in our custom made hardware which has STM32F429 controller.Thread is disconnecting while debugging & writing & reading operation not succeed.Can you please explain the all steps in...

SGupt.5 by Associate II
  • 762 Views
  • 0 replies
  • 0 kudos