STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32L010K8 TIM2_CH4 PWM can't go to PB1

A'm using LL libraty. I need simple PWM output on PB1.TIM2 init related to CH1 and PA5 work.When I change setup to CH4 and PB1 pwm doesn't go to the pin.Both PA and PB ar clocked.Under debuger I checked MODER registers, AF_5 function is selected.Work...

Kansio by Associate II
  • 5088 Views
  • 8 replies
  • 0 kudos

stm32f030 programming using stm32 flash loader

hi every one.I want to program an stm32f030 chip using stm32 flash loader. I know this programmer communicates with the boot program of the MCU. I used this programmer for a microcontroller of mine in a custom designed board (which has been programed...

AKhor.1 by Associate II
  • 2491 Views
  • 2 replies
  • 0 kudos

STM32F0 CubeMx SPI HAL Driver Initial Pin Level

Hi there, I created a project with STM32F042G6 chip using CubeMX. I am interfacing this IC to another chip using SPI. When I set the SPI1 and try to send a command, just before sending a command I have SCLK, MOSI, and MISO levels are high. After send...

DAkka by Associate
  • 1437 Views
  • 2 replies
  • 0 kudos

STM32H745 Data share

Hi I'm new to dual core programming. I need to share data from M7 core to M4 core and M4 core to M7 core. Can you please let me know the steps I need to start.?

TWalp.1 by Associate II
  • 2833 Views
  • 5 replies
  • 0 kudos

STM32H743ZI2 CAN message receive issue with MCP2551

I have hooked up a STM32H743ZI2 Nucleo board with a CAN tranceiver MCP2551 following the instructions kindly provided by mr. Hudak (https://os.mbed.com/users/hudakz/code/CAN_Hello/) with the exception of replacing the second board with a USB-CAN-modu...

SAmpi.1 by Associate
  • 2709 Views
  • 3 replies
  • 0 kudos

Issue with the STM32H735-DK, OSPI Hyperram

Hi, in the example for the OSPI-memorymapped example, the test procedure is as follows..// This is running fine on the DEV board, ( it also works in byte mode fine.) while (1) { /* Intensive Access ---------------------------------------------...

Naldr.1 by Associate
  • 1711 Views
  • 3 replies
  • 0 kudos