STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

What best for 10 analog input and 20 digital ouput (2 row of 10 output), and additional 2 digital output and 1 digital ouput

There, I am starting this STM32 Board, which I dont know the exact type of STM32 to choose, I need to replacing old machine board (its microprocessor base) with 10 of weight sensor, and 20 stepper motor, and 2 communication and 1 additional output, P...

Siun6 by Associate
  • 963 Views
  • 1 replies
  • 0 kudos

RS485 Uart DMA Tx

I am using stm32f4xx, and I am using UART with DMA normal mode. I have a problem with the Transmit Completed state, When I using the TxCompletedCallbacks I get hard fault error so I learned it does not using with normal mode so I am trying the Transm...

DCtech by Associate II
  • 1660 Views
  • 3 replies
  • 0 kudos

STM32L475 RTC interrupt for every 1s

I want to configure the RTC interrupt for every 1s in L475. Since all RTC interrupt are routed through EXTI, is it possible to generate the interrupt periodically without depending on external signal? Something like second interrupt (SECIE) in STM32F...

PBala.2 by Associate II
  • 1650 Views
  • 2 replies
  • 0 kudos

Resolved! ST’s secure service in STM32H750

We are working with STM32H750VBT6. Our project works with an external QSPI flash. We planned to put our bootloader in STM’s internal flash and our firmware in the QSPI flash. We need to protect the internal flash (bootloader) for reading from the ext...

BEvge.1 by Associate II
  • 1773 Views
  • 2 replies
  • 0 kudos

Reading in ADC on STM32H753

I am trying to run a simple program that can read in data from a potentiometer through ADC. The pot is connected to PF10 or A5 on the nucleo board. My code is below:When I run this it prints "Value is: 32767" once then stops. Because I am in conti...

JWolf.3 by Associate II
  • 1632 Views
  • 1 replies
  • 0 kudos

STM32F429 Discovery Kit LEDs does not blink

Dear STM Community,I am a Fresh learner of STM32 technologies. I got myself an STM32F429 Discovery Kit.As expected, I tried to do Led Blinks on my board since it is the hello world of this technology.However, I couldn't turn on the LEDs on board. I c...

0693W00000BdPLVQA3.jpg 0693W00000BdPLaQAN.jpg 0693W00000BdPLfQAN.jpg 0693W00000BdPPSQA3.jpg
SKAŞ.1 by Associate II
  • 1933 Views
  • 2 replies
  • 0 kudos

What is out put data rate of lis2dh and lis3mdl ?

i read data sheet of lis2dh and lis3mdl. i am using st linux driver to read raw data of accelerometer and magnetometer. Now when i set sampling frequency 1600 for accelerometer i get data of x axis at 40 ms. when i set sampling frequency 80 for ma...

Mpraj.19 by Associate II
  • 895 Views
  • 0 replies
  • 0 kudos

USART1_IRQ HANDLER ISR is not getting executing after enabling RXNEIE is set in cr1 and setting priority in NVIC_ISER1 register in stm32f401re nucleo board.anyinputs?

#include<main.h> #include<stdarg.h> void SystemInit(); void Uart1_config(); void uart_printf(const char *fmt, ...); void delay(int val); void Gpio_Enable(); void USART1_IRQHandler() { uint16_t rx; rx=USART1->DR; GPIOB->ODR ^=1<<3; USART1->...

Nchun.1 by Senior
  • 1532 Views
  • 4 replies
  • 0 kudos