STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! I'm using SPI to communicate with a MIPI chip, the commands to the MIPI are sent as 9 bits but the data sent back is 8 bits.

I'm using SPI to communicate with a MIPI chip, the commands to the MIPI are sent as 9 bits but the data sent back is 8 bits. The 9 bit are set up in a uint16_t variable. Using HAL_SPI_Init the data size is set to 9 bits. When I receive the data using...

WScot.1 by Associate II
  • 3542 Views
  • 6 replies
  • 0 kudos

Which MCU support Capacitive Touch Button and Touch Slider

Hello support,I want to develop one product based on touch button and touch slider.so which STM MCU supports those features.and what are the softwares avaialble to develop firmware for touchand also i need hardware design guide for the same.thanks

MThak.1 by Associate
  • 1362 Views
  • 2 replies
  • 0 kudos

RTC with Internal Crystal - STM32F303CB

Hi,I am trying to use RTC with Internal Crystal, I am not able to initialize the internal crystal of RTC. I am trying to initialize the internal clock by the RCC_CSR_LSION flag but I am not getting the RCC_CSR_LSIRDY flag set by the controller.void R...

Connectiion error

​I am using STM32H743XI(we made board)However, an error occurred when connecting using the existing ST Link v2 product.An error occurred (No debug probe found connected to the USB port Session aborted)​​IAR 8.40.1 using ​The firmware(ST-Link) was als...

BPark.5 by Associate II
  • 1456 Views
  • 2 replies
  • 0 kudos

What best for 10 analog input and 20 digital ouput (2 row of 10 output), and additional 2 digital output and 1 digital ouput

There, I am starting this STM32 Board, which I dont know the exact type of STM32 to choose, I need to replacing old machine board (its microprocessor base) with 10 of weight sensor, and 20 stepper motor, and 2 communication and 1 additional output, P...

Siun6 by Associate
  • 963 Views
  • 1 replies
  • 0 kudos