cancel
Showing results for 
Search instead for 
Did you mean: 

Where is STM32H735G-DK full .hex file as supplied from the factory?

SPefh.1
Associate

There's a file STM32Cube_Demo-STM32H735G-DK-V1.0.0 on the website, but it's not the one referenced in the accompanying .bat file (which has a name ending in "FULL") and seems to just (sometimes) load up the selection screen but mostly gives me a blank screen, and any selection leads to a blank screen.

Is there a documented way to restore the board entirely to factory starting condition?

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
thomfischer
Senior

Hello,

the hex file is ok,

i had to modify "program_hexfile.bat"

it could not load the external loader file, because of the SPACE in "Program Files"

1. changed the path to my programmer directory

2. copy the external loader file "MX25LM51245G_STM32H735G-DK.stldr" from the prgrammer directory to the batch file directory.

3 changed the path of the external loader file in the batch file

...

:: C:\Program Files\STMicroelectronics\STM32Cube\STM32CubeProgrammer-2-6-0\bin\STM32_Programmer_CLI.exe

::@SET STM32_PROGRAMMER_PATH="%ProgramFiles(x86)%\STMicroelectronics\STM32Cube\STM32CubeProgrammer\bin"

@SET STM32_PROGRAMMER_PATH="C:\Program Files\STMicroelectronics\STM32Cube\STM32CubeProgrammer-2-6-0\bin"

...

::@SET STM32_EXT_FLASH_LOADER=%STM32_PROGRAMMER_PATH%\ExternalLoader\%EXT_LOADER2%.stldr

@SET STM32_EXT_FLASH_LOADER=%EXT_LOADER%.stldr

...

then you should get the following output freom the batch file

C:\work\arm\stm32\temp\en.STM32H735G-DK_demo\STM32H735G-DK_demo\Binary>program_hexfile.bat
 
=================================================
Erase and Flash all memories and reboot the board
=================================================
 
      -------------------------------------------------------------------
                       STM32CubeProgrammer v2.6.0
      -------------------------------------------------------------------
 
ST-LINK SN  : 002700373438510C34313939
ST-LINK FW  : V3J7M2
Board       : STM32H735G-DK
Voltage     : 3.31V
SWD freq    : 24000 KHz
Connect mode: Under Reset
Reset mode  : Hardware reset
Device ID   : 0x483
Revision ID : Rev Z
Device name : STM32H72x/STM32H73x
Flash size  : 1 MBytes
Device type : MCU
Device CPU  : Cortex-M7
 
 
Mass erase ...
 
Mass erase successfully achieved
 
 
Memory Programming ...
Opening and parsing file: STM32Cube_Demo-STM32H735G-DK-V1.0.0.hex
  File          : STM32Cube_Demo-STM32H735G-DK-V1.0.0.hex
  Size          : 31505827 Bytes
  Address       : 0x08000000
 
 
Erasing memory corresponding to segment 0:
Erasing internal memory sector 0
Erasing memory corresponding to segment 1:
Erasing internal memory sectors [4 7]
Erasing memory corresponding to segment 2:
Erasing external memory sectors [0 45]
Erasing memory corresponding to segment 3:
Erasing external memory sectors [128 140]
Erasing memory corresponding to segment 4:
Erasing external memory sector 144
Erasing memory corresponding to segment 5:
Erasing external memory sectors [144 147]
Erasing memory corresponding to segment 6:
Erasing external memory sectors [176 587]
Download in Progress:
██████████████████████████████████████████████████ 100%
 
File download complete
Time elapsed during download operation: 00:02:39.826
 
Hard reset is performed
 
C:\work\arm\stm32\temp\en.STM32H735G-DK_demo\STM32H735G-DK_demo\Binary>
 
 

if you have still problems, post the batch file output

SPefh.1
Associate

Thanks!

Still doesn't work from the bat file for some reason, but I got it to work by selecting the correct loader, erasing and programming it directly from the programmer (and putting SW1 in the right position).

   -------------------------------------------------------------------

            STM32CubeProgrammer v2.5.0

   -------------------------------------------------------------------

ST-LINK SN : 003300213438510734313939

ST-LINK FW : V3J7M2

Board    : STM32H735G

Voltage   : 3.28V

SWD freq  : 24000 KHz

Connect mode: Under Reset

Reset mode : Hardware reset

Device ID  : 0x483

Revision ID : Rev Z

Device name : STM32H72x/STM32H73x

Flash size : 1 MBytes

Device type : MCU

Device CPU : Cortex-M7

Mass erase ...

Error: Mass erase operation failed.

Please verify flash protection

Memory Programming ...

Opening and parsing file: STM32Cube_Demo-STM32H735G-DK-V1.0.0.hex

 File     : STM32Cube_Demo-STM32H735G-DK-V1.0.0.hex

 Size     : 31505827 Bytes

 Address    : 0x08000000

Erasing memory corresponding to segment 0:

Erasing internal memory sector 0

Erasing memory corresponding to segment 1:

Erasing internal memory sectors [4 7]

Erasing memory corresponding to segment 2:

Erasing external memory sectors [0 45]

Error: failed to erase memory

Error: failed to erase memory

Hard reset is performed