cancel
Showing results for 
Search instead for 
Did you mean: 

Is it possible to reset the CM4 from the CM7 on the STM32H747?

Embedded123
Associate

Or at least make software reset work on only one core?

Thanks

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Imen.D
ST Employee

Hello @Embedded123​ 

Welcome to the STM32 Community =)

It is possible to disable BOOT_CM4 option bit (see "FLASH option bytes" section in the reference manual RM0399)

You can use STM32CubeProgrammer to disable the CM4 in the option bytes.

Imen

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen
Embedded123
Associate

Hi Imen,

Thank you for your answer.

If I understand well, you are proposing a way to disable the CM4 from booting after a reset/power up?

I have code running on both cores. I'm trying to find a way to reset one from the other. Is there a way to do that?

Thank you!