STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

My F3Discovery board is not recognised.

On my f3 discovery board, i was measuring voltage between 5v pin and GND with multi meter and the power LED started blinking . When i removed the the multimeter i noticed the com LED is turned off and the board disappeared from ports in device manage...

0693W00000D23IdQAJ.png
asim khan by Associate III
  • 1573 Views
  • 2 replies
  • 0 kudos

RM0440, Rev 6, STM32G4 Reference Manual - Errors

Figure 151, Page 682: The second line in the picture should be "ADC Master EOC".Section 27.5.68, Page 1054: Description for bit 20 ADCTBRST should be similar to bit 14. Currently, it is a circular reference to itself "Refer to ADC3TBRST description."...

How to disable JTAG on STM32H743XIH6?

Hello there, we're using STM32H743XIH6 MCU for out development.We're at a stage where, we need JTAG to be disabled for Production build and enabled for the Debug build.In order to do that, I searched online, and figured that RDP level can be set to d...

JJ1 by Associate II
  • 4206 Views
  • 3 replies
  • 0 kudos

Resolved! STM32G0 USART wakeup implementation for an existing HAL project

Hi,Months ago I developed a complete project using HAL libraries for the STM32G030K8T microprocessor. Now I need to implement a low power (STOP0) mode and wake-up it from deep sleep using USART. The point is I am facing the following problems:My proj...

Gaston by Senior
  • 1097 Views
  • 1 replies
  • 0 kudos

Modbus RTU crc calculation- STM32F407

Hi everybody,First, I'm sorry for my poor English.I'm using STM32F407VET6 and I want to calculate 16bit CRC of Modbus RTU. Can anybody help me how I can use hardware CRC of the STM32F407? Is it possible to use hardware crc for modbus rtu? Or should I...

mh2 by Associate III
  • 2574 Views
  • 4 replies
  • 0 kudos