For some time, microcontrollers ST have not been available on the market. The lead time is of the order of 6-8 months. Suppliers do not guarantee deliveries. When will the situation return to normal?Thanks.
I have a demoboard STM32H735-DK. I develop a demo for my customer. All OK. But when I supply the card (with USB cable) the application-firmware doesn't run: I have to press the button reset for start it. Why? Thanks for your answer.
Great!Thanks Tesla DeLorean!!!!!With your suggestions the issue is solved; now the STM32H735-DK works correctly.I switch the SW1 to System Memory, in this modality I could connected with ST-LInk and I deleted the flash.Than I switch SW1 to "flash" an...
Hi Mike.The JP7 is in position 1-2 (power from ST-Link) and switch SW1 is in position 0 ("Flash").I have already tried to connect under reset but the connection is not established
Hi.For me, the USB cable is ok because with other board it works correctly.The power source is the USBThe LD5 and LD6 are ONWith ST-Link Upgrade Utilities I can connected to ST-LINK V3 (inside on the board STM32H735-DK) and upgrade it to last version...
Hi.I have implemented a demo for a client using STM32H735-DK. For me, this is the first experience with graphic. I created the project starting from the touchgfx templates. All worked correctly!But now I have to design the custom board with some diff...
The same thing happened to me too.With an STM32H735-DK. One day, I turn on it but it didn't run. The integrated ST-Link V3 seems to work correctly (I can connect it to the PC) but the STM32H735 does work: it not run and I cannot program it. The d...