STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

[STM32F3] HSE crystal selection, confused by AN2867

I'm trying to select a suitable HSE and size the capacitors + resistor for it following the procedures laid out in AN2867, but I can only reach a "not compatible" result even with the example values used in there (the different stages are done for di...

Jopj by Associate II
  • 2747 Views
  • 2 replies
  • 0 kudos

STM32L412 RAM Issue

Hello Folks,Im working on STM32l412kb uc (40 kb RAM Size) .My code uses 32kb of data still we have 8KB RAM.But there is one issue with our results i.e stack size overflow we dont get desired output that is only due to stack size overflow.We also o...

PM.4 by Associate
  • 1761 Views
  • 2 replies
  • 0 kudos

STM32F072RB discovery board The STM32 in slave mode is to be used to read sensor data at every 2 second interval by an ESP8266 master through I2C. I am using the HAL library for this.

The I2C interrupts were enabled and HAL_I2C_Slave_Receive_IT() and HAL_I2C_Slave_Transmit_IT() functions were called. The slave can receive and transmit the data only once and then it pulls the SCL line low disabling further communications. I have tr...

SD.7 by Associate
  • 1064 Views
  • 1 replies
  • 0 kudos

UART receive interrupt issue HAL_UART_Receive_IT remains BUSY

Hi ,I am using HAL_UART_Receive_IT(UART_HandleTypeDef *huart, uint8_t *pData, uint16_t Size) HAL api for uart receive interrupti am calling it at end of HAL_UART_RxCpltCallback(UART_HandleTypeDef *huart)it works for some time but after some time HAL_...

SA.17 by Associate III
  • 5700 Views
  • 9 replies
  • 0 kudos

I would to generate option byte file in hex format

@Exmple::020000041FFFDC:01F800000007:020000041FFFDC:01F80200FF06:020000041FFFDC:01F80400FF04:020000041FFFDC:01F80600FF02:020000041FFFDC:01F80800FF00:020000041FFFDC:01F80A00FFFE:020000041FFFDC:01F80C00FFFC:020000041FFFDC:01F80E00FFFA:00000001FFI was a...

Vikas1 by Associate
  • 1287 Views
  • 3 replies
  • 0 kudos

Resolved! Is there a replacement for the STM32F4 discovery kit?

I am starting a project which involves a CMOS camera. I only need to take still images, not video. I would greatly prefer being able to use a microcontroller over an SBC or FPGA. STMicro used to have an STM32F4 with a camera daughter card, but it app...

JSmit.30 by Associate
  • 1253 Views
  • 2 replies
  • 0 kudos

RTC subsecond alarm wake from STOP

I am building an application that requires maximum power efficiency. We have decided to use an STM32L031K6 MCU. Our application requires waking up at specific times to power on other external devices. Because the system sleep times can range from ...

NHui.1 by Associate
  • 1052 Views
  • 1 replies
  • 0 kudos