cancel
Showing results for 
Search instead for 
Did you mean: 

External clock for STWIN data adquisition

JQ.2
Associate

Hello friends of STM. I am new to STM32 MCUs, and I am working on a project using the STWIN. I have another Data Adquisition Card that is programmed to output a clock signal when I send a command or press a button. I would like to datalog the signals from this DAQ synced to my STWIN. For this task I have to modify the example "HSDATALOG" of the STWIN, in order to change the way it uses the clock for datalogging tasks, so it can take an external clock as an input via GPIO. My priority is to save the data from the analog mic IMP23ABS. I have read for several hours the documentation and the code on the IDE, but I am still very confused because there are many clocks, and too many functions. Can you please help me guiding me on this task?

Thank you in advance

Jacobo.

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0