STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How to read data correctly from NEO-6M GPS module?

Hi.I am trying to read data from the GPS module using USART1 and then send to to a serial monitor through USART2. It ended up not printing the information correctly on the serial monitor. (I have tried to connect the GPS module to a FTDI module direc...

0693W00000D1pAQQAZ.png
M7890.1 by Associate III
  • 6676 Views
  • 12 replies
  • 0 kudos

I cannot obtain any design resources regarding PFC/DPS, st-pld, st-wds, which neither provides open source code nor can I visit www.biricha.com.

I am designing PFC & DPS using STM32G474, I also bought a NUCLEO discovery kit, but I cannot obtain any design resources regarding PFC/DPS, st-pld, st-wds, which neither provides open source code nor can I visit www.biricha.com. And I believe www.bir...

HXU.1 by Associate
  • 1679 Views
  • 3 replies
  • 0 kudos

Resolved! Logins Broken By New Password Rules

There doesn't seem to be anywhere to post issues with the forum itself?I couldn't login this morning - the site kept saying my password was wrong.I know that it wasn't wrong, because I copy it from a password manager.So I had to do a password reset.T...

SWD Data Trace timestamp 0

Hi there,when I try to log my ADC data with the SWD Data Trace I can see every write access to my variable but the timestamp becomes 0 after the fourth sample. Attached is a screan shot to show what I mean. After quite a while the <cycles> tap switch...

0693W00000D2XUAQA3.png
LGard.1 by Associate II
  • 790 Views
  • 0 replies
  • 0 kudos

I2C commands to LCD

I am learning this new 32-bit from my 8-bit world as well as new IDE on top of re-learning C. So be gentle....I am trying to use the CubeIDE to talk to an I2C LCD. I am following a tutorial but the LCD does not respond at all.Some of the code below...

SScot.3 by Associate II
  • 11296 Views
  • 17 replies
  • 0 kudos

Resolved! STM32 UART on android

How to connect to UART via USB on android device? Do I need some driver on android device?​Stm32L432KC nucleo​

oeliks by Senior
  • 2383 Views
  • 3 replies
  • 0 kudos

float values of array are not assigned during a for loop

I want to convert a bunch of uint16_t values from an ADC into floating point voltages. For this I use a for loop to loop through the uint16_t array and write the values to a float array. But the float array remains 0 as if no assignment is ever made....

0693W00000D2U7SQAV.png 0693W00000D2U7XQAV.png 0693W00000D2U7cQAF.png
Mnemocron by Associate III
  • 4395 Views
  • 6 replies
  • 0 kudos

Fast Timer Interrupt Distrupts My Program

I need to achieve fast interrupts because I'm making integration from accelerometer and gyroscope datas in my code. And when I set a timer interrupt frequency to 2.5ms code get stuck. But when I increase timer frequency to 25ms it works just fine. ...

IAtam.1 by Associate II
  • 2058 Views
  • 4 replies
  • 0 kudos

We would appreciate your support to provide us with the current lifecycle status (e.g., Active, NRND, to be discontinued (LTB), Obsolete, Custom) for this part (STM32F107VCT7TR).

Greetings,SiliconExpert is contracted by Cicor Technologies Ltd to work with their suppliers for accuracy and compliance purposes.We would appreciate your support to provide us with the current lifecycle status (e.g., Active, NRND, to be discontinued...