STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Any Microchip KSZ example code for stm32h7 processor

We are working with KSZ8563 3 port ethernet switch over the RMII interface. Communication is MDIO and it is working. But we couldn't run the lwip udp example.Is there any sample software on KSZ Phys, so I will check the settings? Our controller is ST...

umtkyck by Associate II
  • 3385 Views
  • 3 replies
  • 0 kudos

Interrupts I2C

Good afternoon everyone!I hope you are well. I happen to be new to handling STM32 and I want to generate an interrupt with I2C, CAN ANYONE HELP ME WITH THAT?I just need to know what functions I need and how I generate the interrupt routine.I have a S...

JGóme.1 by Associate II
  • 1033 Views
  • 1 replies
  • 0 kudos

Resolved! Can you write values to the RTC counter registers(RTC_CNTL/RTC_CNTH) after you've set them to an intial value?

I've been trying to implement a clock and calendar into my solar tracker project(using an stm32f103) so that I can set at which time it should go to sleep ( and for how long) , but every time the board goes into standby the counter -unfortunately- ge...

HAbay.1 by Associate III
  • 1684 Views
  • 3 replies
  • 0 kudos

Resolved! ERROR common.c: addr too high

I am getting this error after I modify my linker script (which I got from a project created with CubeIde):$arm-none-eabi-objcopy -O binary Prog_test_H735.elf Prog_test_H735.bin$arm-none-eabi-size Prog_test_H735.elf  text     data      bss      dec  ...

ERhod.1 by Associate II
  • 4150 Views
  • 8 replies
  • 0 kudos

Resolved! Bootloader information discrepancy

Reference Manual for STM32H72xxx/73xxx (RM0468), section 2.6, says that the embedded bootloader can be accessed via I2C1, I2C2, I2C3, I2C4 and SPI1, SPI2, SPI3, SPI4, however AN2606 only lists I2C1, I2C2, I2C3 and SPI, SPI3 as the working I2C and SPI...

HWidj.2 by Associate III
  • 1627 Views
  • 2 replies
  • 1 kudos

Error finishing flash operation

I have the following error when I was trying to debug using TrueStudio(v9.3.0).​The specific steps that caused the error are as follows.1. Connect STM32F100RB※1 to the PC.2. Launch TrueStudio(v9.3.0)3. make project 3.1 [File] -> [New] -> [C Projet] 3...

0693W00000D2PylQAF.png
Myasu.1 by Senior
  • 1321 Views
  • 1 replies
  • 0 kudos

Resolved! STM32L052 USART: Problem Switchover from Output- to UART - TX - functionality produces a disturbing H/L - edge on TX

Two Usart - TX - lines shall be used either in PP- output- or in Usart - TX - mode.The switchover from a normal output pin to a Uart - TX - pin produces an High/ Low edge on TX followed by an interrupt on TX side.On RX- side this H/L edge causes an ...

FEber.1 by Associate III
  • 2221 Views
  • 4 replies
  • 0 kudos

FDCAN confusion

Hello,I hate to say this, but I am completely lost in regards to programming FDCAN to receive extended ID messages from an ECU. I looked to the examples provided in the IDE as well as other questions on this forum, but am still confused. I have a str...

Aaronium by Associate III
  • 1084 Views
  • 1 replies
  • 0 kudos