User Activity

There appears to be very long lead times for this product. Any reason and is there any chance it will get better?​
I am successfully using a timer and DMA to capture 4096 samples from ADCs 1 & 2 using a master slave configuration on a STM32H747- Disco board.I would really like to simultaneously capture 3 channels. Is it possible to capture samples from ADC 3 usin...
I have been using the MSC_Standalone example to develop code on this DISCO board. I noticed that although the example makes use of the on board display, it only uses the top half. Is there a good reason for this and is there an easy fix to use the wh...
Help! I have been experimenting with STM32CubeIDE and a STM32H747i-Disco board for a few weeks now. All was going well, I was able to compile, modify and debug code. Then something went wrong and I had to re-install STM32CubeIDE, now I can't seem to ...
The function int32_t BSP_SD_Init(uint32_t Instance) (which I believe is the first thing to call to initialise access to the SD card on the STM32H747 Disco board) attempts to check if card detected on line 160. However the pin that is used as card det...
Kudos from