STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F469I-DISCO standby mode RTC wake up immediately issue.

Posted on February 12, 2018 at 07:12I used STM32F469I-DISCO and STM32F429I-DISCO to testing Standby mode function by PWR example(Attach). Standby mode function is no problem on STM32F429I-DISCO.  But in STM32F469I-DISCO , used RTC wake up form stand...

Hank Lee by Associate II
  • 3680 Views
  • 8 replies
  • 1 kudos

I2C on STM32L151CC dies intermittently

I have a tilt sensor KX112 connected to the STM32L151CC on I2C2. It seems to work fine but at times the I2C bus comes up as busy and the sensor cannot be read. Rebooting the board solves the problem for a while but it crops up again. I am running th...

PGogt by Associate III
  • 3765 Views
  • 7 replies
  • 0 kudos

STM32H7, Clock MX Functions to Cube(.ioc project creation)

I have working external clock source HSE system clock configuration, now wanted to change to HSI (internal clock).But simply changing to HSI will not fix all the Multipliers and dividers to get same frequency output. Is there way to import the System...

YSN by Senior
  • 897 Views
  • 2 replies
  • 0 kudos

STM32F411VE, Problems with SDcard unavailable while using SPI

HI,​I am using the STM32F411E-DISCO board.and, I'm going to read the image from SDcard and deliver it to FT800 by SPI.​The problems that have occurred are as follows.If I use SPI without SDIO, FT800 works normally.If I only use SDIO, I can read and w...

Slee.61 by Associate
  • 1299 Views
  • 2 replies
  • 0 kudos