Hello everyone,I would like to implement a basic spi communication with an sx1276 transceiver using CM4 as master in standalone mode in order to get the chip id. The spi5 configuration has been done using stm32cubeide which is the way i did it with a...
Hello, i would like to know why after st-link programer has been cut-off usart1(pa9,pa10) and usart3(pb10,pb11) doesn't work at all.Any help would be appreciated.Thanks
Thanks for the prompt reply.For now, i don't have any probe to test with.The board is powered with 5V on E5V and i've also done some tests with 3V but none of them work.I don't know where or what to look for.