STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Switching Port Pins between Alt Function and Normal mode

Hi All,In a situation where someone might be flashing an LED using a Timer Output (eg Alternate Function Mode connected to a Timer channel output), what if you want to then turn the LED on solid or totally off and then maybe back to the Timer flashin...

RMyer.1 by Associate III
  • 2579 Views
  • 6 replies
  • 0 kudos

STM32H747 HSEM issue

Hello,I am trying to manage data transfer between the 2 core of the STM32H747.My problem is all hardware semaphore are locked just at the initialisation phase ( MASTERID 0X03 , Core M7) After Hal_Init(); & SystemClock_Config(); all is free.after __HA...

Configuring OCTOSPI on a STM32H723/STM32H730

I'm having an issue configuring the OCTOSPI for accessing an external HyperRAM (Cypress S27KL0643) connected to OCTOSPI1.My basic issue is that the STM32 doesn't provide a chip select or clock when I attempt to access the chip.I'm suspect I'm misconf...

0693W00000DqN0KQAV.png
JCoop.2 by Associate
  • 3436 Views
  • 4 replies
  • 0 kudos

Resolved! Stm32f427vit6 replacement

Can i replace the stm32f427vit6 with the f429vit6, f437vit6 or 439vit6 without changing code, and are they completely pin compatible?​​​

DSmit.111 by Associate II
  • 1656 Views
  • 2 replies
  • 0 kudos

Flashing large binary (> 1Mb) to STM32H753VIT not working

Hello everyone,For over a year I've been involved in a project using the STM32H753VIT microcontroller. The firmware has been in development for quite a while and has subsequently been growing.Currently, the compiled binary is at the point where it is...

0693W00000D1NukQAF.png 0693W00000D1NxZQAV.png
GtH by Associate
  • 5539 Views
  • 9 replies
  • 3 kudos

How to configure 32kHz LSE oscillator via HAL?

I think I've set up everything sensibly via STM32CubeMX to get HAL control of the LSE, but the external oscillator appears to be not operable. In particular, there is essentially no voltage on the 32kHz crystal pins, so of course it will not oscillat...

FMC for STM32 in muxed mode

Please help me with operation of the FMC module in STM32F407VE. It is necessary to connect external RAM memory; since FMC module in this microcontroller uses the address bus and data bus in muxed mode, its need to demultiplex this signals. For this p...

Kvon .1 by Associate
  • 2908 Views
  • 1 replies
  • 0 kudos