STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! ADC of STM32F401RC sometimes do not work

Hi,I configure the ADC as the following code; but sometimes(not everytime) the code will run to Line 70 : "Beer_Out_Dis(1);" ,and ADC will not work.Did I do something wrong? Thanks verymuch./* ADC1 init function */ static void MX_ADC1_Init(void) {   ...

Pzhu.1 by Associate II
  • 1610 Views
  • 2 replies
  • 0 kudos

Resolved! How to solve the problem with: 1. " Error: No STM32 target found!". 2. "Error in final launch sequence: Failed to start GDB server Failed to start GDB server Error in initializing ST-LINK device. Reason: (4) No device found on target."

--The first error encounters while trying to connect the board (STM32H7A3ZI-Q) with STM32Cube Programmer at normal mode.--The second error encounters while trying to upload a code through STM32Cube IDE. However, when I try to connect the boa...

0693W00000D0ZRiQAN.png 0693W00000D0ZRYQA3.png 0693W00000D0ZRTQA3.png
PWaiba by Associate II
  • 4329 Views
  • 5 replies
  • 0 kudos

Bank Swap

There is a point that confuses me, I am reading from the datasheet, but I wanted to ask some questions.For stm32f4, there is FB_MODE bit in the SYSCFG register (8th bit), if the FB_MODE bit is 0, the address 0x08000000 becomes BANK1, if it is 1, the ...

DCtech by Associate II
  • 958 Views
  • 1 replies
  • 0 kudos

Octo-SPI memory-mapped mode speed for H735

Hi,We are using the OCTOSPI2 on a H735 in memory map mode.We are copying 32 bits values one by one, from the internal RAM to the Octo memory.We transfer around 5000 x 32 bits in 2ms which is around 10MB/s.I think, it is a bit slow. What is the maximu...

Resolved! Using OCTOSPI in Memory Mapped mode with an QuadSPI SRAM

Hi guys,I am using an STM32L552ZET6 and I would like to extend the RAM using an external SRAM chip (23A1024-E/TS), that has an QuadSPI interface. I would like to know if I can use STM32L5 OCTOSPI interface in memory mapped mode with the above mention...

CDan.1 by Associate II
  • 1934 Views
  • 3 replies
  • 0 kudos

STM32F103 upper flash pages corrupted/erased.

Dear ST community,I was wondering if you could help me with a problem I'm having with an STM32. I have a system containing an STM32F103VET6. The last flash pages are used to store settings/parameters. 2 redundant flash pages are used. This system...