STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How to use the crypto library on M4-core of the STM32H757?

Hi,I tried to use the crypto library "STM32CryptographicV3.1.1_STM32H7_IARv8_otnsc.a" on the M4-core of the STM32H757 but I got some troubles as explain below. First of all, I'm using IAR 9.10 and I haven't problem when using the library on M7-core. ...

Byann.1 by Associate II
  • 4588 Views
  • 7 replies
  • 0 kudos

motionstudio2 window application connection error

I tried connecting the bno080 with nucleo 411RE using motionstudio2 window application to read the data from bno080.....I saved the flash memory for running this application and flashed the stm with another program...I flashed the application running...

AR.7 by Associate II
  • 925 Views
  • 0 replies
  • 0 kudos

how to measure force of motor

i need to measure force of a motor but i don't know i how to measure .please any one help me i'm using 24v dc motor with encoderand stm32f446re controller

LOGU by Associate II
  • 1423 Views
  • 2 replies
  • 0 kudos

c++ project in keil IDE

Hi,I'm trying to write some c++ code in keil for stm32. I have successfully written C code that compiled well but I can't create a c++ project.anyone has experience with it?

EPora.1 by Associate II
  • 822 Views
  • 0 replies
  • 0 kudos

Program Download and verification issue

Hello,I am using STM32F746BGT6I am trying for LED toggling.I am using cube programmer for downloading hex. I am facing verification issue, but download was successful. After download complete, i reset my controller. But my toggle logic is not working...

Mani1 by Associate II
  • 1975 Views
  • 3 replies
  • 0 kudos

STM32F103 Cann't use SPI3 CLK with Debug Mode.

Hello?I'm use STM32F103 RCT6 SPI3 with EEPROM.But When I use IAR Debug. can't read or Write. because no have clk  Without IAR Debug // SPI3 Config /////////////////////////////////////////////////////////////////void SPI3_Config(void){ SPI_Init...

0693W00000DlYHCQA3.png 0693W00000DlYHMQA3.png 0693W00000DlYHRQA3.png

Read flow rate sensor with STM32F411RE Nucleo - Timer Interrupts

I have a water flow rate sensor which I want to read with my STM32F411RE Nucleo-64 board. The output signal is a frequency. How can I read the signal? The sensor has following properties:Flow Range = 1 - 15 L/minPulses per Liter = 2200Frequency Outpu...

As.2 by Associate II
  • 3395 Views
  • 5 replies
  • 0 kudos