User Activity

Hai:I am using STMcube IDE 1.13.2 and TouchGFX 4.22.1 in my project. Once flash the program to the traget, If i given play but program not run. Once i press the RESET button or Power ON and OFF then it will work.This happend only in 1.13.2 IDE versio...
Hi,I am using STM32F407VET6 IC to measure 3 Phase AC voltage,Phase Angle, Frequency PF,Current.now i am trying to measure AC voltage using ADC,(stepping down AC voltage and measuring the voltage with ADC by sampling and averaging).and Timer channel i...
Hai :I am using STM32H7 MCU custom board with Hardware Buttons. Set points can be changed by selecting the menu in the menu list and using the button.What the option used in the Touchgfx framework? I am trying change menu selection(Highlights). So us...
Hai.....,I am using STM32H743IIT6 custom Board and CubeIDE. Run the code after download it showing "Target not responding retrying......." and again try to download the same code in MCU i couldn't download, It show "Error in initializing ST-LINK de...
Hai,we are using STM32H743IIT6 and External Twin quad spi (MT25TL01G).In our board we have configured (PB6) pin for QUADSPI_BK1_NCSbut in the external loader file(MT25TL01G_STM32H743I-EVAL.stldr) which we have has PG6 pin for QUADSPI_BK1_NCSDue to th...