STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Question regarding FFTs in arm_math.h

Hello! I am trying to simulate an octave model on a microcontroller and ran into a snag I thought I'd get some help with. So I have an FFT I am running on a sample of data (we'll say 4096 bytes). In octave, I'm using an FFT of the sample (where the s...

JayDev by Senior II
  • 6432 Views
  • 8 replies
  • 0 kudos

Boot0 pin on STM32L011 has internal pull resistor?

Hello all.I'm using BOOT0-PB9 pin on a STM32L011. In the reference manual I've found that "The pin logic level can then be read as an input value on the shared GPIO pin.", but nothing about internal pull resistor.The question is: is this pin provided...

hi iam trying to find FFT using stm32F4 discovery board. i have tried using CFFT and RFFT available in arm CMSIS DSP library but iam getting wrong answers. Can someone please tell me where iam wrong. Iam posting the code below for both RFFT and CFFT ?

-----------------------------------------------------------------*/ #include "main.h" #include "usb_host.h"   /* Private includes ----------------------------------------------------------*/ /* USER CODE BEGIN Includes */ #define ARM_MATH_CM4   #incl...

Vk.2 by Associate II
  • 1202 Views
  • 0 replies
  • 0 kudos

Resolved! UART RECEIVE PROBLEM / STM32G061C6

Hi all,I am using a STM32G061C6T6 MCU. I'm trying to contact Nextion HMI. My data sending is successful, but I can't get any data. I couldn't run any of the Pooling and interrupt methods when receiving data. When I follow the RX pin with the oscillos...

0693W00000DmdEtQAJ.png

Communication via RS485 stop working after random time

Hi everybody,This is the first time I'm writing in a forum so I'm sorry if I didn't right.I'm developed a board based on STM32F091VBT.I'm using this board to communicate with other devices (two touch, a gateway and another board based on STM32F091VBT...

JDame.1 by Associate
  • 3151 Views
  • 2 replies
  • 0 kudos

RTC clocks problem

Something is wrong with the clocking and i cant figure out. When i try to debug with step over, the error handler in void SystemClock_Config(void) if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK) {  Error_Handler(); }Takes me to    /* Wait till L...

0693W00000DmdaaQAB.png
asim khan by Associate III
  • 2120 Views
  • 3 replies
  • 0 kudos

Please give me some example for RS485 with automatic hardware flow control when interfacing with Energymeter...Tried a lot but not able to receive anything from energymeter.

I have connected my RS485 automatic hardware flow control with energymeter and with the help of that, tried to transmit the query 01 04 00 21 00 02 (forf voltage) along with CRC check ....uint16_t ModRtu_CRC(uint8_t buf[8], int len){ uint16_t crc = 0...

SVerm.3 by Associate III
  • 2369 Views
  • 1 replies
  • 1 kudos