STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

SPI 3-wire bidirectional master not sending clocks

I have an issue with SPI in bidirectional mode (MOSI, CLK and CS). I have a device which I need to write to and from. When I have to write to an adress in the slave device, it works perfectly: reg=0x04; CS_DRIVER_LOW c=HAL_SPI_Transmit_DMA(&hspi2,...

MRey.1 by Associate III
  • 3344 Views
  • 7 replies
  • 0 kudos

Interrupts and internalFLASH access results in CPU stallment

We experience a stalled CPU when accessing (writing) the internal FLASH memorySTM32L432KBUFreeRTOStaskENTER_CRITICAL(); __HAL_FLASH_CLEAR_FLAG(FLASH_FLAG_EOP | FLASH_FLAG_OPERR | FLASH_FLAG_PROGERR | FLASH_FLAG_WRPERR | FLASH_FLAG_PGAERR | FLASH_FLA...

MMits.1 by Associate II
  • 4703 Views
  • 10 replies
  • 0 kudos

stm32f4 TIM2 multiple channel input capture

Hello,I'm trying to write a PWM input capture function(I only need the on time. not the frq and duty cycle) and I see that it takes two channels of a timer. I need to use all four channels, Is it possible?Thanks

EPora.1 by Associate II
  • 6606 Views
  • 10 replies
  • 0 kudos

I'm using X-CUBE-SFXS2LP1 with STM32CubeIDE ("Easy portability across different MCU families, thanks to STM32Cube"). It has examples for NUCLEO-L073RZ, NUCLEO-L152RE or NUCLEO-L476RG, but I want to use something else. How do I do it?

X-CUBE-SFXS2LP1 is the S2-LP Sigfox expansion library for STM32Cube.There are no STM32CubeMX configuration files in the projects included in X-CUBE-SFXS2LP1, so how can I modify the MCU, GPIO pins, etc.? Maybe I'm missing a feature of STM32CubeIDE fo...

jallen by Associate
  • 1542 Views
  • 1 replies
  • 0 kudos

Dual bank issue on a STM32F769BG.

 Hello,I work on a STM32F769BG and I m currently trying to setup the dual bank. I have a bootloader that check the validity of the application on the current bank and an application. My bootloader works in single bank configuration however it doesn't...

RRaph.1 by Associate
  • 1310 Views
  • 1 replies
  • 0 kudos

SPI2 Communication on STM32H743X

I have been using STM32H743x for a project. There i use SPI2 to communicate with a serial flash IC.I need different packet sizes when accessing the Flash. The problem i have is, when i change the TSIZE at different stages, the firmware freezes at the...

SFons.1 by Associate II
  • 1715 Views
  • 2 replies
  • 0 kudos

Resolved! USB virtual com port can't receive data when device reboot

Hello,​I experienced a phenomenon in which the USB port was not reconnected.This phenomenon occurs when a USB port is connected to the product and reboots.​I check my device manager. When i turn off product, com port also disappear.and product reboot...

0693W00000Dmc7wQAB.png
hjuns by Associate III
  • 2147 Views
  • 4 replies
  • 0 kudos