STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! We're programming STM32F302 chip and getting an "unable to get core ID" failure. We've used the following hardware successfully numerous times on various PC's with success. Any ideas why this isn't working? Hardware setup in detials.

•STMicro programmerhttps://www.digikey.com/en/products/detail/stmicroelectronics/STLINKV3MINI/10266291?s=N4IgTCBcDaIMoBUAyBJAcgaQLQDUDMAsuiiALoC%2BQA•Programmer cablehttps://www.tag-connect.com/product/tc2030-ctx-stdc14-for-use-with-stm32-processors-...

Ybelf.1 by Associate
  • 8992 Views
  • 2 replies
  • 0 kudos

Did my STM32L496 Disco arrive with broken internal settings?

Hello,I have recently purchased an STM32L496 Discovery Kit to play around with and get familiar with the chip. I have decided to start porting some of my OS from a different board to this board, but before I even got to that stage I ran into some iss...

FBisk.1 by Associate II
  • 3633 Views
  • 6 replies
  • 1 kudos

SPI block on SPI_WaitFlagStateUntilTimeout

HI all,I have a custom board with stm32h743vit6 microController.I configurated SPI1 for comunicate with a SPI display (ili9488 managed by touchgfx with partial frame mode).My problem is that I can't reach high speed (more than 25mhz on SPI) else the ...

MPast.1 by Senior II
  • 2185 Views
  • 3 replies
  • 0 kudos

CubeMX & FreeRTOS -> Using SysTick

Posted on March 31, 2016 at 12:11Hello I'd just like to know why CubeMX strongly recommends to use other timers besides SysTick as source? I've always thought that the SysTick timer is basically intended for use with an embedded OS? Thanks

STM32L562E-DK VCP UART. TX OK. RX NO

Hello, guys!My name is Luis and I bought the board STM32L562E-DK for testing purposes for a new project.I have been executing many examples based on freertos and I am very happy on how the STM32L562Q could be my solution in a future project.However, ...

Llope.3 by Associate
  • 3507 Views
  • 3 replies
  • 0 kudos

MODBUS ERROR-RS485 Converter_ Reg

Hi, I am having data transfer problem with Modbus only when I use a specific RS485 Converter .I am using STM32H750VB as my main IC for a fuel dispenser project. I am having a problem with my MODBUS based on the RS485 converter.i)If i am using...

FDCAN with stm32h7451z in CLASSICAL FRAME mode

Hi there,I have problems when I m using the FDCAN controller. I m using the NUcleo STM32h745ZI with a shield with a can controller on in CLASSICAL CAN mode (NO FDCAN).If a run an example in the HAL_Driver folder it works ( @1MHz Fdcan kern freq = 40M...

DVicc.1 by Associate II
  • 1473 Views
  • 1 replies
  • 0 kudos