STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

SAI config for I2S microphones

Hello. I'm looking for information on how to configure I2S microphones using the SAI peripheral. I'm using H743, but this likely applies to any SAIL-capable STM32. The Reference manual, and an application note discuss PDM microphone setup in detail, ...

DOCon.1 by Senior
  • 1530 Views
  • 0 replies
  • 0 kudos

Resolved! Is it normal to have a long and irregular LSE startup time?

I am using the STM32L151 processor.I noticed that the LSE takes between 140ms and 712ms to get ready RCC_FLAG_LSERDY. I think Is a time of 700ms still a correct time? Fluctuations are normal?code:while ((uint16_t)RCC_GetFlagStatus(RCC_FLAG_LSERDY) ==...

JHuls.1 by Associate
  • 2097 Views
  • 3 replies
  • 0 kudos

Resolved! DMA keep sending data

Hi all,I want to send 3 bytes with the UART DMA controllerbut when this line is executed, the uart sends these 3 bytes endlessly .Why does the transmitting not stop after 3 bytes ?HAL_UART_Transmit_DMA(&huart1,(uint8_t *)spi_buf_in,3);Thank youSteve

sde c.1 by Senior II
  • 1221 Views
  • 3 replies
  • 0 kudos

How to read chip id and unique id STM32L462REY

Hello, I want to read the chip ID and unique id by using SPI but I cannot read. I am using an external library, ( https://github.com/nimaltd/w25qxx for flash ) You can find my cube documents in the attachments below. What should I do? Thank you.

luplupp by Associate
  • 4994 Views
  • 4 replies
  • 0 kudos

STM32 MCU powering the peripherals by VBAT

Currently we are looking for the possible approach for Switching between Main supply (LDO) and Vbat Operation. We have Two backup supplies requirement , Battery and supercap. Either one of the backup supplies is selected but provision should be provi...

SSiva.11 by Associate
  • 4412 Views
  • 2 replies
  • 0 kudos