STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Can't connect to target STM32f105RC.

Hello Community!I was using a system controlled with the STM32f105RC, I was able to program it with the ST-Link. In that system I got a problem so I had to change to another board with the same characteristics but, when I did so, I wasn't able to pro...

OBorr.1 by Associate II
  • 2169 Views
  • 1 replies
  • 0 kudos

Is FT5426 similar to Ft5336

HI, I am using a custom board where i need to devlop a touch driver. I am using FT5426.I have the complete code of fT5336 as it was used in STM32f746-disco board.can i just by changing the register AND CONFIGURING the i2c pins accordingly.make the to...

Mselv by Associate II
  • 1514 Views
  • 1 replies
  • 0 kudos

STM32H7A3 and 5" LCD with ST7701

I'm using STM32H7A3 16bit RGB+3wireSPI to a 5" LCD with ST7701. I plan to use STM32H7A3's LTDC function. Where do I find sample codes to display basic shapes on LCD? .h file for ST7701 registers is also helpful.Thanks.

JNguyen by Senior
  • 2081 Views
  • 1 replies
  • 0 kudos

Resolved! STM32L5 - User Option Byte Access

The STM32L5 reference manual states that there are "4 Kbytes of option bytes for user configuration" accessible via the Flash register interface (section 6.3.1), but no further details are provided on how to access that space for user data storage.I ...

MBand.3 by Associate III
  • 4858 Views
  • 2 replies
  • 0 kudos