STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Using Sparkfun Arduino Qwiic Shield with STM32H7451-DISCO

I am attempting to drive some I2C 5.0v / 3.3v peripherals via the Sparkfun Arduino Qwiic Shield connected to an STM32H7451-DISCO.I can't seem to raise the devices on the I2C bus despite being able to communicate with the audio codec and LCD which are...

SNort.1 by Associate II
  • 2122 Views
  • 3 replies
  • 0 kudos

Can I work this process minimum 750 Hz in Nucleo L432?

Hello. For a project, I need to read 4 channels analog data and save them in to the sd card for 10 seconds. I should record every data minimum with 750 Hz. And then I generate pwm signal with these data. I tried that but it was not successful, recor...

MÇeli.2 by Associate II
  • 1798 Views
  • 3 replies
  • 0 kudos

DMA vs BDMA

HiI want to use spi6 on stm32h7 controller in DMA mode, i see i can use BDMA instead of DMA. looking at the reference manual, i see following about BDMA"The BDMA is used to perform programmable data transfers between memory-mapped peripherals and/or ...

DGupt by Associate III
  • 8030 Views
  • 4 replies
  • 0 kudos

Resolved! High-frequency square wave using timer not possible?

Hi,I'm trying to see what the maximal frequency I can achieve using the STM32F407-discovery board.So far I have found the following:using TIM1 Internal clock (168MHz)Output pin PE9If i put the period at 1000, I get the following result:However if I p...

0693W00000FDmVmQAL.png 0693W00000FDmW1QAL.png
MDrac.1 by Associate III
  • 15981 Views
  • 4 replies
  • 0 kudos