STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32L432KCU6 ADC returns incorrect values

Hello everyone,For a project I'm working on, I'm using the STM32L432KCU6 MCU. After writing some code I've managed to make the STM32L432KCU6 do what I want/need, except that the ADC returns incorrect values from some of the ADC inputs.In this project...

J.dW by Associate II
  • 5861 Views
  • 6 replies
  • 0 kudos

Stream Buffer on STM32Fx?

Hi everyone!Somebody here has a basic example for stream buffers on a single core devices? Preferably with use of interrupts.Thanks a lot!

by Not applicable
  • 1114 Views
  • 3 replies
  • 0 kudos

Resolved! How to work with radians?

How to work with radians in HAL? I include a math library #include "math.h" and trying to implement a formula which has radians cleansignal = 3.0 * sin (radians (Count)); And CubeIDE gives me an error: undefined reference to` radians'

DK.7 by Senior
  • 1493 Views
  • 1 replies
  • 0 kudos

Resolved! How to for loop question??

I have what I am sure to most a simple C question (I'm a hardware guy at this end).....For brevity I would like to take the following statements and combine them using 1 for loop but don't know the semantics on how to do this....I am using the HAL li...

SWenn.1 by Senior III
  • 2478 Views
  • 6 replies
  • 0 kudos

Sending IR datas via timer

Hi,I have STM32G0 series MCU. I want to receive and send IR datas. I can receive IR datas successfully with timer via DMA. and then I want to send these datas as IR datas.I try to use 2 channels. I set one channel as output compare no output for timi...

fozen.1 by Associate
  • 1029 Views
  • 1 replies
  • 0 kudos

STM32F103C8T6 SP1 and TIM3 PWM doesn't work together

Hi, I have a strange problem here, I configure SPI1 as Half duplex master and configure the unused MISO pin to TIM3 PWM Generation CH1. But as soon as I initialize SPI1 PWM stops working. I looked up the performance block diagram they're not even on ...

e-zeki by Associate III
  • 1788 Views
  • 2 replies
  • 0 kudos

Resolved! Problem with generating PVM with DMA

Hello, I need to learn how to control an LED. Faced a problem while trying to generate PVM with DMA. I suspect the error lies in the initialization of the DMA. After running the code, no signals are observed. It was based on the project, which is con...

DalOpez by Associate II
  • 5753 Views
  • 10 replies
  • 0 kudos