STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32 ADC not working?

Ive been trying to get active passthrough between my adc and dac from pa1 and pa0 respectively. Ive confirmed all my functions are being called but i just cant seem to get any value loaded into my DAC. if i give it a value manually, i get the correct...

plsWork by Associate II
  • 1121 Views
  • 1 replies
  • 1 kudos

Resolved! How to read state of SYS WKUP pin ?

I am using the  Nucleo-L433RC-P board and have configured pin PC13 as SYS WKUP (for the blue top button).How can I read the state of this pin when the processor wakes up, because HAL_GPIO_ReadPin will not work.I am sure I used a function or macro to ...

Interrupt curiosity (STM32G491)

Hello friends : )I've recently tested the NUCLEO-G491RE board for an upcoming redesign.Current design relies on quite tough interrupt latency so here is where I begun.As I understand, with no FPU usage (in isr) (ASPEN + LSPEN = 0) one could expect up...

Reset pin - add external pullup, or not?

Hello team,Generally , Reset pin by default status is Logic High.But in AN4206 ( Page 31) , NRST pin is not Connected to 3.3V , it is left Floating with Capacitor.Is that Okay ? My device is STM32F303.Regards,

bsuthar by Senior
  • 1463 Views
  • 9 replies
  • 1 kudos

USB CDC minimum working example for STM32C071?

Apologies for the ignorance, I'm a beginner with STM32 and I purchased the STM32C071K8T6 MCU since it has built-in USB capabilities. I am trying to implement USB CDC, but I'm becoming quite confused with all the USBX and ThreadX stuff I have to enabl...

Resolved! NUCLEO-N657X0-Q STM32CubeIDE NetXDuo

Hi everyone, for several days I've been trying to replicate the Nx_TCP_Echo_Server application example by creating a project with the .IOC file, but I can't establish Ethernet communication. If I compile and run the example, everything works, but m...

GEKO by Associate II
  • 953 Views
  • 4 replies
  • 1 kudos

STM32F746BGT6 (LQFP208) 10" LCD Flickering Issue

Hi Folks,I’m currently observing flickering on a 10" TFT LCD screen and would appreciate some expert advice regarding the connections for LCD_CLK, LCD_HSYNC, and LCD_VSYNC.At present, the signals are connected as follows:MCU LCD_CLK → Non-Inverting B...

hari0369 by Associate
  • 359 Views
  • 1 replies
  • 1 kudos