STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

RCC_DBP flag set timeout

Hi, I have a low power controller which i will use as RTC.type: STM32L031F6P7.I use a custom boardThese are the clock settings  I also notice there is no oscillating signal at PC15 . When should the LSE oscillator start? after powerup or after System...

0693W00000GZDpfQAH.png 0693W00000GZ5FFQA1.png 0693W00000GZDpkQAH.png
sde c.1 by Senior II
  • 1048 Views
  • 1 replies
  • 1 kudos

STM32H7 RTC BKUP registers issue

HiWe are using the STM32H7A3ZIT6 for one of our irrigation controllers that we are developing. To check the "power cuts" time, we always save the RTC value (uint_32 seconds value) before voltage goes down, using:HAL_PWR_EnableBkUpAccess();HAL_RTCEx_B...

Resolved! Hello, I am facing a issue to generate generate a external clock from MCU on MCO1 GPIO pin on STM32F769I Discovery board.

Here are the details on MCO1 pin configurations, GPIO_InitStruct.Pin = LL_GPIO_PIN_8; GPIO_InitStruct.Mode = LL_GPIO_MODE_ALTERNATE; GPIO_InitStruct.Speed = LL_GPIO_SPEED_FREQ_HIGH; GPIO_InitStruct.OutputType = LL_GPIO_OUTPUT_PUSHPULL; GPIO_InitStruc...

STM32H7 dual core - M4 SPI Issue

After configuring SPI channel on the M4 core as a read only master (while observing signals on the scope) I was not able to generate a clock while using the  HAL_SPI_Receive() functions (which returned HAL_ERROR status). When I changed the configurat...

yuri CH by Senior
  • 1033 Views
  • 1 replies
  • 0 kudos

how to use just Rx pin of an uart

Hi, I have a sensor that send data over uart to a stm32f722 uC. This sensor is powered at the same time of uC. I've noticed that some times the sensor stop sending data. For example, if the code is running ok and then reboot the uC some times the sen...

Lgarb.1 by Associate II
  • 3266 Views
  • 2 replies
  • 0 kudos

STM32F767ZI UART DMA RX LOCK(STOP)

After system initialization, UART DMA Rx function is normal.When time passes, data is not received in the DMA buffer and the phenomenon is stopped.To solve the problem, we checked the normal operation by repeating the DMA initialization as shown belo...

Snam.2 by Associate
  • 2420 Views
  • 4 replies
  • 0 kudos