User Activity

Hello,I am writing a custom bootloader for STM32L4P5RET6 largely based on the "How to Create a Super Simple Bootloader" videos:https://www.youtube.com/watch?v=OkUQ3iMmiYQWhen beginning, I was using CubeIDE 1.9.0 and whatever was the latest FW for the...
I am posting the support ticket here as well, because it took six weeks to get a first response to the original support ticket.It is likely related to the issue reported in this posting:https://community.st.com/s/question/0D53W00000raYd2SAE/intermitt...
Hello,I'm trying to understand which steps need to be taken when exiting the stop modes with STM32L4R7ZIT.Say that we are in stop1 mode, RCC->CFGR-STOPWUCK == 0 (MSI). Before entering stop1 we were clocked by HSE 12 MHz via the main PLL into 120 MHz ...
Hello,Does anybody know if there is any prerequisite when enabling or disabling the prefetch buffer?More specifically, in the Nucleo L4R5ZI sleep example the prefetch buffer is disabled in main() just before the main loop. It is never re-enabled afte...
Kudos from